Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the meaning of Quantum analog input module 140ACI04000 isolation of 1780V between channel and bus.
Isolation between channel to Bus @1780V AC means that quantum backplane bus will be protected upto 1780V AC for 1min generated through channel(field) .

Channel: Channel is the terminal where field connection to be terminated.
Bus: Bus is a backplane bus circuitry where module is connected to get energize its circuit.

Isolation voltage i.e. 1780V will be not displayed anywhere, it is a internal component phenomenon to protect the circuit in case of over voltage.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings