Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
170INT11000 Interbus module report red lit in RD Led. What is the cause of this behavior.
The Red RD LED means that the sensed network I/O and the configuration does not match. You must have all the I/O-bus network I/O cards mapped correctly and installed for the remote bus to run. Before the CPU starts the remote bus it will compare the I/O map to what is physically connected. If there is a difference the I/O will be disabled and the Red RD LED illuminated on all of the I/O-bus modules. This will also occur if any of the cables are broken, disconnected, or if a base fails. This also means that you cannot preconfigure I/O in the I/O map for future expansion or have any I/O bases on the bus that are not mapped.
If error is intermittent then could be a problem of loose connection and any INT module might have some trouble.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings