Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the use of Parallel Kit for SRC5000UXI to 10000UXI models?
The Parallel Kit allows to connect the two UPS's output supply to the load through a common AC bus bar.
Both the UPS's will share the load equally when both the UPS's are working fine.
But if one UPS should fails, either through developing a fault or being taken out for maintenance, then the load will work on the other UPS.
’1+1’ parallel redundancy system is available to effectively improve the reliability of the system.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings