Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When selecting a target to develop a project for standard PC, which target should be selected there is no selection for standard PC.
To see the Standard PC in target you need the Vijeo designer development to be licensed. If it is licensed then you can see one update button on Help--> About under License Tab.

Click on update and put the code VJDHTGTSPV62M for version 6.2 and click ok.

You will see Generic Windows PC series in target to create application to be downloaded in Standard PC.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings