Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will Altivar 71 drive automatically reduce the switching frequency in case of temperature rise.
The Drive is able to modulate the switching frequency, in function of the thermal state. If the thermal state is too high the drive will automatically reduce the switching frequency. To simplify, the temperature level is determined by the drive with measuring the heat sink temperature.
Above 2.5, 4 or 12 kHz, depending on the rating, the drive will reduce the switching frequency automatically in the event of an excessive temperature rise.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings