Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In the CPU configuration for Quantum CPU in Unity Pro, what is the meaning of "Data Storage" and why it is used.
The data storage is used for READ_U_PCMCIA and WRITE_U_PCMCIA function blocks.

Lets say for e.g.. you configure the Data storage size as 2000 kB then the 2000 kB of data storage represents:

2000 kiloBytes * 1024 = 2048000 Bytes

Since The READ_U_PCMCIA and WRITE_U_PCMCIA functions are working with word addresses:

So 2048000 Bytes / 2 = 1024000 Words

Hence Addresses from 0 to 1024000 for the memory card can be used for data storage.

In the MAST section of the program, program as follows:
The memory card is connected into slot 0.
The WRITE_U_PCMCIA function writes 10 words to address 10000 on the memory card from %MW100.
The READ_U_PCMCIA reads 10 words from address 10000 on the memory card to %MW110.

​Representation of WRITE_U_PCMCIA and READ_U_PCMCIA in ST language:
WRITE_U_PCMCIA (0,10000,10,100,Status_write);
READ_U_PCMCIA (0,10000,10,110,Status_read);


Basically The WRITE_U_PCMCIA function transfers data from the PLC RAM memory to the user memory card archiving zone and The READ_U_PCMCIA function transfers data from the user memory card archiving zone to the PLC RAM memory. The function READ_U_PCMCIA allows addressing the PLC zone's beginning to be copied to the PCMCIA card up to 65 535.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings