Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Configure the number of battery strings using NMC terminal mode in Smart-UPS SRC1000ICCIND / SRC1000UXIND ?
Connect the serial cable to the serial com port on rear side of UPS.
1. Open a terminal program, such as HyperTerminal™.
From the Desktop, go to: Start, Programs, Accessories, Communication, HyperTerminal
2. Follow the prompts to choose a name and select an icon. If the message, "...must install a modem,” click
Cancel.
3. Go to File, Properties. Select the COM port that is connected to your UPS. The port settings are:
– bits per second - 2400
– data - bits 8
– parity - none
– stop bit - 1
– flow control - none
4. Click OK in each of two windows
5. Press ENTER to initiate connection to UPS.

1. Once the blank terminal window is open:
2. Press ENTER to initiate terminal mode. Press ENTER multiple times, until the prompt
User Name: is displayed. Follow the prompts. Type slowly, waiting until each character appears on the
screen prior to typing the next character.
Network Management Card defaults:
– User Name: apc
– Password: apc
3. Press 1 and ENTER to select Device Manager.
Select the model by entering the corresponding number, then press ENTER.
4. Press 3 and ENTER to select Configuration.
5. Press 1 and ENTER to select Battery.
6. Press 2 and ENTER to change Battery Settings.
7. Type in the number of battery strings then press ENTER.
8. Press 3 and ENTER to accept the changes.
9. Press ESC five times to return to the main menu.
10. Press 4 and ENTER to log out.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings