Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Configure the number of battery strings using UPS terminal mode in Smart-UPS SRC1000ICCIND / SRC1000UXIND ? "
Connect the serial cable to the serial port on the back of the UPS. If using USB communication to the UPS,
disconnect USB cable prior to connecting serial cable.
1. Open a terminal program, such as HyperTerminal
From the Desktop, go to: Start, Programs, Accessories, Communication, HyperTerminal
2. Follow the prompts to choose a name and select an icon. Disregard the message, "...must install a modem”
if it is displayed. Click Cancel
3. Go to File, Properties. Select the COM port that is connected to your UPS. The port settings are:
– bits per second - 2400
– data - bits 8
– parity - none
– stop bit - 1
– flow control - none
4. Click OK in each of two windows
5. Press ENTER

1. Once the blank terminal window is open, follow these steps to enter the number of battery strings:
NOTE: Letter key commands are case sensitive. Use capital letters when using letter key commands.
2. Press Y. The UPS will respond with SM in the command box. If the UPS does not respond to the Y
command, ensure the serial cable is securely connected to the serial port on the UPS. Use only an APC by
Schneider Electric supplied serial cable.
3. When SM appears in the command box press the > key. The UPS will respond with the number of battery
strings connected to the UPS. If the UPS has not been previously programmed to recognize the number of
battery strings this number will be zero.
4. Use the + or - keys to change the number of battery strings. OK will appear in the command box.
5. Press > key. The number of battery strings will appear in the command box.
NOTE: The + or - keys and the > key must be used again to change the number of battery strings from this
point in the programming.
6. Press R. The UPS will respond with BYE in the command box.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings