Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can ATS48 Soft Starter generate power feed-back.

In steady state and regenerative mode, the motor is in hypersynchronous so the energy is sent back to the main, with no problems.
The problem can be if you have a low current (close to the PHF threshold) and during the transition between motor/generator state then the residual current can be only the magnetizing current and decrease under the PHF threshold.
No energy is transferred during deceleration.
Only a little during deceleration in dynamic braking stop mode but do not take this into account because it is a very low level of energy.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings