Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
We are not able to add more than one rack and BMXNOM0200 module with BMXP342020 in the configuration.
With BMXP342020 CPU version 1.0 it will supports only one rack in the topology and also NOM module also not supported with this version.
For BMX P34 20X0 with OS version 2.0 or higher supports 4 Racks maximum.
To use NOM module with BMX P34 20X0 cpu then maintain the minimum version of CPU OS to 2.10.




Schneider Electric India
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
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings