Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we move holding registers to input registers in Unity Pro.
Yes , we can use "WRITE_INPUT_INT"  EF for moving holding registers to input registers but considered the 3X register should not be mapped on IO module or somewhere in configuration to avoid any conflict .

Restrictions with WRITE_INPUT_INT:
  • The function block provides access to one variable at a time (elementary data types and not arrays of elementary data types).
  • Only variable addresses are allowed, you cannot use declared variables even if they are mapped on a %IW direct address.
  • The simulation block WRITE_INPUT_INT does not work if the I/O module is configured in a RIO rack but works properly if the I/O module is configured in a local or DIO rack.

Schneider Electric India
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
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings