The error message " PLC return error code FDH-83,80H" is due to the Magelis reading the discrete/analog inputs as %I from the Unity Quantum. Quantum only support reading Input in Located SRAM data location not directly from %I or %IW.
To resolve the error you will need to delete the tags and link to the Unity database file. Then re-link the tags back into Vijeo Designer and check the box to "force IO to unlocated variables". Or convert all of the input variables to memory bits and words. I suggested that he use the MOVE_AREBOOL_INT function block to move the inputs to a memory word.
To resolve the error you will need to delete the tags and link to the Unity database file. Then re-link the tags back into Vijeo Designer and check the box to "force IO to unlocated variables". Or convert all of the input variables to memory bits and words. I suggested that he use the MOVE_AREBOOL_INT function block to move the inputs to a memory word.
Released for: Schneider Electric India