Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What will be the reason of output current unbalancing on ATV71 drive.
For output current unbalancing of the drive please check the following:--

(1) Please check & tightens the cable connection at motor and drive side.

(2) Make it confirms; cable size is same for all 3 output phases, as impedance network can cause unbalance of output current.

(3) How to check: --
=> Example, R=120 A, Y=100 A & B=90A.
The first test to do=> is to know if the problem comes from the ATV or from the Load side (i.e. Motor, cables). This can be done if you inverse R and Y and perform the measurement of current. If the current in R becomes equal to 100 A and the current in Y is 120 A, it means that the problem comes from the Load side.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings