Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to use single Altivar 71 drive on two motors with one encoder in FVC mode (closed loop).
Yes, It is possible to use the encoder with 2 motors in parallel but only if the 2 motors are MECHANICALLY CONNECTED (rigid connection and not by belt for example) and the motors are identical.
In this case encoder check on encoder is possible.
Please note that, if one motor is changed or rewinding we can't guarantee the good working

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings