Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between the I/O mode and separate mode in the Altivar71 drive.
The difference between the I/O mode and separate mode is the means to control the drive:
- In separate mode the reference and the command can be sent via 2 different channel but follow the DriveCom chart. For example you have to do a sequence before start the drive i.e. to send CMD=16#0006, then CMD=16#0007 and then CMD=16#000F.

- In I/O mode only one bit of the command word can run the drive. In this mode we are working with a virtual I/O terminal. Each bit of the command word can be used to enable a function (Start, stop, forward, reverse...).

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings