Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Controller inside card VW3A3501 Battery lifetime is 8 years, is there any alarm when to change battery.
There is no function, which give an alarm when the battery is out of order.
It is possible to check by the program if the battery is ok or not. Declare a variable as "RETAIN" and initialize it with a value (the value is saved in the controller inside board after a shutdown).
Check it in your program and if the value is 0 after a shutdown, it means that the battery is dead.

Schneider Electric India
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
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings