Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Recover From a Lost Password in Netbotz 200?
Please follow below mentioned steps for recovering from lost password :

Use a local computer connected to the Main Module to access the control console.
1. Select a serial port at the local computer; disable any service that uses the port.
2. Connect the serial cable (APC part number 940-0024 or 940-1524) to the selected port on the computer and to the RS-232 Console Port at the Main Module.
3. Run a terminal program (such as HyperTerminal) on your computer and configure the selected port to have 9600 bps, 8 data bits, no parity, 1 stop bit, and no flow control.
4. Press ENTER, repeatedly if necessary, to display the User Name prompt. If you are unable to display the User Name prompt, verify the following:
• The serial port is not in use by another application.
• The terminal settings are correct as specified in step 3.
• The correct cable is being used as specified in step 2.
5. Press the Reset button on the front of the Main Module. The Status LED will flash alternately orange and green. Press the Reset button a second time immediately while the LED is flashing to reset the user name and password to
their defaults temporarily.
6. Press ENTER as many times as necessary to redisplay the User Name prompt, then use the default, apc, for the user name and password. (If you take longer
than 30 seconds to log on after the User Name prompt is redisplayed, you must repeat step 5 and log on again.)
7. From the Control Console menu, select System, then User Manager.
8. Select Administrator, and change the User Name and Password settings, both of which are now defined as apc.
9. Select Accept changes.
10. Press CTRL+C, log off, reconnect any serial cable you disconnected, and restart any service you disabled.

Schneider Electric India
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
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings