Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between TSXP571634 and the TSXP571634M.

Article available in these languages: Thai

The TSXP571634 and the TSXP571634M are the same Premium CPUs. They have the same specifications. The "M" at the end of the part number only indicates multi-language documentation.

For coated version add C at the end of the reference: example TSXP571634M becomes TSXP571634MC.

If Product reference is without any Suffix then no documentation will be provided with the Product.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings