Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to program Analog Output to output frequency on ATV71 drive.
There is only one Analog Output (AO1) on ATV71 drive without option card.

Program following in [ INPUTS / OUTPUTS CFG] (I-O-) Menu;

- AO1 [AO1 assignment] to [Motor freq.] (OFr): Output frequency, from 0 to [Max frequency] (tFr).
- AO1t [AO1 Type] to [Voltage] (10U): Voltage output
- UOL1 [AO1 min Output] to 0 V
- UOH1 [AO1 max Output] to 10.0 V

You will get 10V between AO1 & COM when Output frequency is max frequency (tFr).

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings