There is no channel level diagnostic available for 140DDI35300 and 140DDO35300 but yes we can read the health status of the complete module by using system word from %SW180 to %SW339. The address can be selected as per the module position. Refer to Unity pro Help for details.
Released for: Schneider Electric India