Minimum version required/recommended to update Quantum from Concept to Unity:
Quantum PV
140CPU43412A/B >=04
140CPU53414A/B >=04
CPUs with PV < 04 include RAM Memory chip whose characteristics are not totally adapted to the Unity program execution.
According to the used memory size, these CPUs can work in Unity range but can also present defects in case of Online changes, configuration changes or programs size increase.
The consequences that can have are:
- No start of the CPU
- Some modules are not working in the configuration.
Quantum PV
140CPU43412A/B >=04
140CPU53414A/B >=04
CPUs with PV < 04 include RAM Memory chip whose characteristics are not totally adapted to the Unity program execution.
According to the used memory size, these CPUs can work in Unity range but can also present defects in case of Online changes, configuration changes or programs size increase.
The consequences that can have are:
- No start of the CPU
- Some modules are not working in the configuration.
Released for: Schneider Electric India