Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is OPF1 fault on ATV71 drive.
OPF1 is the output phase loss fault.
This fault appears when one motor phase is loss on the output of the drive
The minimum time to detect one motor phase loss is 500ms.
The threshold by phase is: I (U,V,W)< Drive nominal current /4 during ODT ( Output phase loss detection time ).

Remedy:
(1) Check the connections between the drive and motor.
(2) Depending on the application type and the motor setting, increase Odt[OutPh time detect] parameter.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings