Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is No Load Shutdown in Bx1100CI-in .
The no load shutdown feature works when the Battery Saver mode is enabled and the Back-UPS is in the On Battery mode. The Back-UPS will shutdown if the connected load draws less than 30 W of power for more than 5 minutes. Disable Battery Saver mode if only low power consuming equipment like ADSL-modem or wi-fi router is connected to the Back-UPS.

Schneider Electric India

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings