Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Derating factor to be considered when Masterpact 4 Pole breaker is used in AC Application with 2 Pole connected in parallel.
Derating factor to be considered:

For Two poles in parallel when used in AC Application

-Reduction factor of carrying current: 0,9 (each pole can carry 0,9 In, not In)

-Breaker Current Carrying Capacity; 1,8 x In (instead of 2 x In)

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings