Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we access M340 or M580 CPU remotely through PMXNOW0300 module.
Yes, it is possible to access M340 or M580 CPU remotely by using Acksys PMXNOW0300 module.

In PMXNOW0300, there are 3 ports available with auto-sensing 10/100 Base TX and auto MDI-MDIX network interface.
One port is reserved for the M340/M580 CPU or M340/M580 NOE connection.
When connected to the M340/M580 native Ethernet port, PMXNOW0300 ports are considered as “Slave”.
If connected to the M340/M580 NOE Ethernet port instead, PMXNOW0300 ports are considered as “Master”, distributed I/O operation is then fully supported (I/O Scanner).

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings