Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we use Memory Card of M340 CPU in M580 BMEH58x040 CPU.
Memory Cards used in the M340 CPUs are not compatible with the M580 CPUs.

Use only a BMXRMS004GPF memory card in your CPU. It is a 4 GB, Class A card rated for industrial use.

If you insert an incompatible SD memory card, then power up the CPU:
  • The CPU remains in NOCONF state.
  • The CPU BACKUP LED turns ON.
  • The memory card access LED remains OFF

NOTE: The BMXRMS004GPF memory card is formatted specifically for the M580 CPUs. If you use this card with another CPU or tool, the card may not be recognized.

Schneider Electric India
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
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings