P 100 [Motor voltage] will be around 415V maximum if parameter F701 is 1.
The average of the 3 phases of line to line output voltages displayed either
in volts or as a percentage of the drive's rated output voltage (200 V for208/240 V models - 400 V for 480 V models). Select % or volts with parameter [Unit value selection] (F701).
Released for: Schneider Electric India