The data on the memory card can be transferred to the device if the data on the memory card matches the device(device type, motor type, firmware version), but the parameter values are different or same.
Refer the below conditions and flow of data exchange of memory card & drive
Released for: Schneider Electric India