170FNT11001 is a Fipio communication adapter to integrate FIP device to master controllers like premium.
The 170 FNT 110 01 Fipio communicator establishes the interface between the Fipio bus, controlled by a Premium PLC and an input/output base from the Momentum product range.
The communicator is compatible with all Momentum catalog connection bases. It can only be used when connected to a base.
The 170 FNT 110 01 Fipio communicator establishes the interface between the Fipio bus, controlled by a Premium PLC and an input/output base from the Momentum product range.
The communicator is compatible with all Momentum catalog connection bases. It can only be used when connected to a base.
Released for: Schneider Electric India