Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Unable to access Rack PDU AP7921B over the web interface ?
Please follow the procedure to check the connectivity.                                                                                                                                                                                                                                                        • Verify that HTTP or HTTPS access is enabled.
•Make sure you are specifying the correct URL — one that is consistent
with the security system used by the Rack PDU. SSL requires https, not
http, at the beginning of the URL.
• Verify that you can ping the Rack PDU.
• Verify that you are using a Web browser supported for the Rack PDU.
See “Supported Web Browsers” on page 85.
• If the Rack PDU has just restarted and SSL security is being set up, the
Rack PDU may be generating a server certificate. The Rack PDU can
take up to one minute to create this certificate, and the SSL server is not
available during that time.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings