Braking resistor switch on voltage is fixed by hardware and it is not configurable in LXM32.
For LXM32___M2 range threshold is 430 vdc if parameter DCbus_compat = 0 (default) and 395 vdc if parameter DCbus_compat = 1
For LXM32___N4 range threshold is 780 vdc irrespective of parameter DCbus_compat settings.
For LXM32___M2 range threshold is 430 vdc if parameter DCbus_compat = 0 (default) and 395 vdc if parameter DCbus_compat = 1
For LXM32___N4 range threshold is 780 vdc irrespective of parameter DCbus_compat settings.
Released for: Schneider Electric India