Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Use of Front port of MCS025 Module of Sepam
Refer the attached Image of front face of MCS025 Module.
The Front port of MCS025 is not meant to use, you should not use it or connect it using any cables. Yes it resembles like the front port of Sepam Base module but not to use for any purpose.
To set the MCS025 we should use the front port of the Sepam base module only.
.

Schneider Electric India

Attachment(s)
MCS025 Module.jpg [11.87 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings