Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How we can perform cold start during power cycle of M340 CPU.
Cold Start: Cold start refers to starting the CPU from power off, Current configuration is discarded and program processing begins again with the initial values.

Warm Start: Warm start refers to restarting the CPU without turning the power off, Program processing starts once again where Retentive data is retained.

Giving power cycle to CPU is not a cold start , however it will be counted as a warm start.

To enable cold start during power cycle, you need to select the cold start only check box in CPU configuration using unity pro software.

Cold Start Only:

If checked, this option forces the cold start of the application, instead of the normal warm start upon power cycle of the PLC.
By default, the Cold Start Only option is unchecked.
The Cold Start Only option is only supported since PLC V2.7

Schneider Electric India
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
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings