Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
UPS BX600C-IN is not working on Generator
Reason for the Problem:

1.Input Voltage/Frequency not in the range.
2.Wave form type is not pure sine wave.
3.Input has noise/distortions[beyond the UPS level of acceptance]
4.Capacity of the generator is less below UPS capacity

Solution:

1.Make sure Input Voltage/Frequency is 230v and 50hz.
2.Wave form type is pure sine wave.
3.No Input noise/distortions.
4.Capacity of the generator should be 1.5 times more than UPS capacity

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings