Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to program ATV630 for quick /immediate stop for the system.

First, program the [Dec. Ramp Adapt] parameter (brA) to "No".

Method 1:
Select Ramp Stop and set the minimum deceleration ramp time (parameter DEC) to a value such as 0.1s (you can adjust DEC as per your requirement).
This will allow the motor to stop in approximately 100 ms, depending on torque and current limitations.
Method 2:
Set the parameter [Type of Stop] (Stt) to [DC Injection].
Then, configure the parameters related to DC injection according to your specific requirements.



Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings