Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the error message E20 / MC1 on AIC VW3A7253.
The error message E20 / MC1 indicates an unknown motor control or power part.
This can happen if the firmware version is incompatible or the power board has an incorrect rating.
When this error message happens during operation both cannot be true. In this case the communication between the control board and the motor control had been interrupted.
The best thing is to change the control block and the motor control board.
Spare part reference: VZ4AAFE1103Y (control block and motor control board together)

Schneider Electric India
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
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings