Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Whether adding these Line choke will “protect” our ATV630 with 100kA system.
There is no need of the line choke for use the ATV630 with 100kA system. The drive has been design for work in the UL condition; The UL require the possibly to mount the product inside cubicle which allow to connect the system at 100kA Isc. Due to the DC choke embedded, the impedance is added on the line and it enough to limit the current on the 100kA system.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings