Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the programming parameter to run ATV71 immediately after switch on the power supply.
Program TCT to LEVEL (LEL) in [1.5 INPUTS / OUTPUTS CFG] (I-O-). menu
If the run command is present. means =>short LI1 and 24V and if sufficient power is available to the drive to power the motor, it will start the motor and allow it to run.
Note: for frequency reference , you need to connect pot for example.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings