Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does BMENOP0300 module supports IO Scanning feature.
BMENOP0300 module doesn't support IO Scanning feature however the BMENOP0300 module supports explicit messaging through the Modbus TCP protocol.
Use the DATA_EXCH function block or WRITE_VAR and READ_VAR function blocks in application logic to create a Modbus TCP explicit message.
NOTE: A single Unity Pro application can contain more than 16 explicit messaging blocks, but only 16 explicit messaging blocks can be active at the same time.

Schneider Electric India
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
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings