Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is reverse input logic in MiCOM P111 relay
Reverse logic means that if an input is energized, the function assigned to this input is disabled. If the input is not energized, the function is enabled.

The logic of the inputs can be reversed: Input L1 to L4 (model A, B) or L1 to L6 (model E).

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings