Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Connection of PTC sensor with ATV320.

If a PTC thermistor is to be used with AV320, connect the COM and DI6 terminals.
At the same time, also the microphone SW2 switch must be set to the PTC position.
Please refer to the attached file.

Schneider Electric India

Attachment(s)
PTC_ATV320.pdf [249.81 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings