Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the default ip address of PTQ-PDPMV1 ethernet port ?
The PTQ-PDPMV1 module is equipped to use an Ethernet connection using the following defaults:
My_ip: 192.168.0.100
Netmask: 255.255.255.0
Gateway: 192.168.0.1
For HSBY units the remote (passive) Master module Ethernet connection is always Primary IP plus 1. For example, Primary IP = 192.168.0.100, Standby module IP = 192.168.0.101.
This setting is not configurable: the module's firmware automatically sets the IP address of the remote (passive) Master.

Schneider Electric India
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
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings