Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to use SPA-ZC 17 with VAMP relays

This is for Vamp 200 relays (not Arc protection) ABB's SPA-ZC 17 is a Bus connection module, which is not powered from the SPA device
(e.g. VAMP relay) but instead it has its own internal power supply. SPA-ZC 17 is normally
connected to a SPA device with a cable which has 9-pin D-connectors in both ends and
direct connection between pins 1, 2, 3, 4, 7 and 9.
When SPA-ZC 17 is connected to a VAMP relay (REMOTE port with TTL interface) the
wire in pin number 4 must be cut.

Schneider Electric India

Attachment(s)
SPA-ZC 17.JPG.jpg [27.46 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings