Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why Surge Suppressors are used in Vamp protection relays.
Surge Suppressors are used to suppress the high voltage spike that is generated when a
relay or contactor coil is de-energized. The electromagnetic field collapsing across the coil
generates a voltage spike in the wires of the control system. Without the suppressor, the
surge can reach value, which is many times greater that rated coil voltage and can
propagate through the system causing electronic controls to go to unwanted operations. In
addition using surge suppressors increases life time of the contactor and control system.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings