Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Max age parameter signifies in Easergy P3 for RSTP configuration
The time during which a configuration message remains valid after being issued by the root bridge. Determines the maximum size of the RSTP network,
also called RSTP diameter. Can be set to max. 40 to allow the largest possible diameter but can be adjusted to improve performance.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings