Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In Unity Pro, can we automatically store the errors generated in diagnostic viewer in a file
It is possible to store in a file all error messages as soon as they appear, disappear or are acknowledged. As soon as a message is read in the diagnostics buffer it is saved in the archive file.
If a fault appears and then disappears, it is represented by a single message in the Diagnostics Viewer (a single line), but by 2 lines in the archive file.
The "Properties" dialog box allows you to activate archiving of error messages. It also allows you to define the type of archiving and the location of the archive file.
Type of archiving
You can choose between 2 types of archiving:
  • cyclic archiving: The history file created is named ProjectName.his, were ProjectName is the name you entered in the "Project Properties" dialog box is.

    in order to avoid the size of the archive file becoming too large, a new ProjectName.his file is created every 1000 saves. The old file then changes name and becomes ProjectName.bak.
    Note: If a ProjectName.bak file already exists, it will be overwritten by the new file of the same name. To avoid a loss of data, you must therefore manage your archive files.
  • periodic archiving: the user defines the frequency with which a new archive file is created (between 1 and 24 hours). The file is created under the name ProjectDraft_date_time (for example, for a file created on 31 July 2001 at 12 h 26 min 55 s: ProjectDraft_073101_122655. If the chosen frequency is 1 h, the next file will be created under the name ProjectDraft_073101_132655, etc.). Creating a new file does not overwrite the previous file.

Schneider Electric India
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
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings