By default, ViewX’s on-screen keyboard is disabled and so users have to interact with ViewX by using a keyboard and mouse.
To enable or disable ViewX’s on-screen keyboard:
- Display the Options Window.
- Select the General tab.
- In the Miscellaneous section, either:
- Check the Enable On-Screen Keyboard check box to make the on-screen keyboard available for relevant displays. Users can now interact with ViewX via devices that do not have physical keyboards.
The keyboard layout varies, depending on the user's Locale settings (Regional Settings for a User in the ClearSCADA).
Or:
- Clear the Enable On-Screen Keyboard check box to disable the on-screen keyboard feature. Users will need to use a physical keyboard to interact with ViewX.
- Check the Enable On-Screen Keyboard check box to make the on-screen keyboard available for relevant displays. Users can now interact with ViewX via devices that do not have physical keyboards.
- Select the OK button to apply the changes.
Released for: Schneider Electric India