The maximum number of BMXNOM0200 modules that can be configured in each X80 drop (with an X80 performance EIO adapter module BMXCRA31210 or BMECRA31210) follow the following rules:
- a maximum of 36 expert channels.
- a maximum of six BMXNOM0200 modules configured.
NOTE: With M580 CPU OS version ≤V2.40, the maximum is limited to four BMXNOM0200 modules configured.
Released for: Schneider Electric India