Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the impact of power outage in BMXCPS4002 and BMXCPS4022.
If the duration of the outage is shorter than the power supply filtering time, it has no effect on the program which continues to run normally.
If the duration of the outage is longer than the power supply filtering time, the program is interrupted and power restoration processing is activated. The CPU then restarts in warm restart or cold start.
The Power Supply Filtering Time of BMXCPS4002 and BMXCPS4022 is ≤ 10 ms.
In case Micro-Power Outage:
Duration <=1/2 period and Repetition >= 1s
The power cut interval time should be larger than 1s
Each power loss time <=1/2 period
Both condition should be fulfilled.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings