Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the relationship between [Frame Recived Timeout] of [ASCII Manager] and [Timeout] of [SEND_RECV_MSG] ?
[Frame Recived Timeout] of [ASCII Manager]
This parameter allows the system to conclude the end of frame at reception after a silence of the specified number of ms.

[Timeout] of [SEND_RECV_MSG]
Here the Exchange timeout is a multiple of 100 ms (0 for infinite) here the timeout refers to the time send recv msg block will wait until it receive the full buffer according to set quantity in sizerecvbuffer.
So if the set time is elapsed then the block will go into error.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings